Advanced Waveform Utility

Impairments Settings

Channel Flatness

Channel Flatness Enabled

User Flatness Profile

AWGN Setup

Enabled

Carrier to Noise Ratio

Carrier Bandwidth

Flat Noise Bandwidth

Channel Flatness

Channel Flatness Enabled

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:CHANnel:FLATness:FILTer[:STATe]ON|OFF|1|0

[:SOURce]:RADio:AWU:WAVeform:IMPairment:CHANnel:FLATness:FILTer[:STATe]?

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.19.03

User Flatness Profile

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:CHANnel:FLATness:FILTer:FILE:NAME

[:SOURce]:RADio:AWU:WAVeform:IMPairment:CHANnel:FLATness:FILTer:FILE:NAME?

State Saved

Yes

Initial S/W Revision

A.19.03

AWGN Setup

This feature allows you to add AWGN (Additive White Gaussian Noise) to a waveform.

Enabled

Enables /disables the AWGN feature.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:STATe ON|OFF|1|0

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:STATe?

Preset

OFF

State Saved

Yes

Range

ON|OFF

Initial S/W Revision

A.19.03

Carrier to Noise Ratio

Set the power boost level of the carrier.

Available only when the AWGN Setup > Enabled checkbox is selected.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:CNRatio<real>

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:CNRatio?

Couplings Only applied when AWGN is enabled.

Preset

0

State Saved

Yes

Min

-100

Max 100
Initial S/W Revision

A.19.03

Carrier Bandwidth

Sets the bandwidth of the applied waveform. As this setting is used to calculate the correct noise power, ensure that this value is the correct bandwidth of applied waveform.

Available only when the AWGN Setup > Enabled checkbox is selected.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:CBWidth <real>

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:CBWidth?

Couplings

Only applied when AWGN is enabled.

When waveform is imported, the max value for Carrier bandwidth is sample rate of waveform/1.25.

Preset

40 MHz

State Saved

Yes

Min

1 Hz

Max 1 GHz
Resolution 1
Initial S/W Revision

A.19.03

Flat Noise Bandwidth

Sets the bandwidth of noise added to the signal. This setting is used to calculate the correct noise power.

Available only when the AWGN Setup > Enabled checkbox is selected.

SCPI Command

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:FNBWidth <real>

[:SOURce]:RADio:AWU:WAVeform:IMPairment:AWGN:FNBWidth?

Couplings

Only applied when AWGN is enabled.

When waveform is imported, the maximum value for Flat Noise Bandwidth is sample rate of waveform/1.25.

Preset

40 MHz

State Saved

Yes

Min

1 Hz

Max 1 GHz
Resolution 1
Initial S/W Revision

A.19.03

Welcome to AWU

AWU Overview

Waveform Settings

Carrier Settings

Segment Settings

Crest Factor Reduction Settings